Change Language :

Plain bearings are crucial components in structures with moving elements. However, even small errors when securing bearings can have serious consequences: unwanted noise, excessive wear or even complete failure of the bearing point. In the following, we will show you the most common causes of these problems, then provide you with suggested solutions and show you how to optimally secure plain bearings.

So-called "drifting" is the reason why we secure plain bearings. But what does this term actually mean?
Drifting plain bearings lose their tight fit in the housing bore and move even though they are supposed to be fixed. This problem often occurs when the press fit - the mechanical tension that holds the bearing firmly in the hole - is insufficient. Causes for this can include:
The plain bearing material expands and is therefore no longer firmly seated in the housing bore.

High loads lead to deformation or creep of the material.

A housing bore that is too large or imprecise will not provide sufficient hold.


Plain bearings that rotate together with the shaft in the hole cause wear in both the housing and themselves. This leads to unwanted noise or even total failure.

If the plain bearings are moved axially or the forces can have an axial effect on the bearing, there is a risk of the bearing moving out of the hole even earlier. In these cases, the bearings must be specially secured in addition to being press-fit. The adjacent table shows the temperature limit above which the plain bearings must be secured in the hole, even at low axial forces. The greater the forces, the more likely it is that such securing should be considered.
If the press fit of the plain bearing is not sufficient, there are various options available for axially securing plain bearings.
The most tried and tested methods are listed below:
The slotted design offers high installation flexibility and compensates for manufacturing tolerances in the hole. The bearing is pressed into place and then it fixes itself automatically. The two flanges ensure that it cannot slip out of the housing bore.
Area of application: Ideal for applications with variable tolerances and simple assembly.
Snap-on bearings have undercuts or locking lugs that compress during assembly and automatically reset after installation to hold the plain bearing securely in the housing.
Application: Useful for manual assembly, as the plain bearings are assembled quickly and efficiently.
In this process, the bearing is mechanically deformed after placement by a flat press so that it sits firmly in the hole.
Area of application: Particularly suitable for high quantities (e.g. automotive industry), as automation offers high precision and efficiency.
Holes in the bearing flange enable fixing with screws. This method ensures maximum holding force, but is complex to assembly.
Area of application: Applications where particularly high forces act or maximum safety is required.
In addition to the locating spigot, the anti-rotation feature is a common design issue. Plain bearings are designed to move through the shaft while the bearing itself is fixed in the housing.
Metal or PTFE plain bearings require a firm fixation, as their sliding properties depend on the liner on the inner diameter. Plastic bearings are more resistant here, as the homogeneous material itself has good sliding properties. Nevertheless, even with plastic bearings, spinning in the hole is undesirable, as housing bores are generally not optimised for friction.
Additional holes in the flange allow screws to be fixed to hold the bearing securely in position. This solution offers maximum stability with low risk of failure, but is cost-intensive for large numbers.

Offsets or undercuts on the outer diameter of the bearing engage in corresponding recesses in the hole. This method is comparatively cost-effective, as it requires almost no additional work during injection moulding.

In some cases, it may be advisable to insert the housing bore in a different way or to change the housing material to enable a better fit for the plain bearing.


Convince yourself of the quality of our products. The iglidur plain bearing sample box contains:
✅ 39 iglidur plain bearings made from the most important materials
✅ Templates for finding the perfect material for your application
✅ iglidur plain bearing technology catalogue with information about our plain bearings

We offer you both special parts and an extensive catalogue product range. This means that you don't always need a special part to secure your bearing. To make your design easier, you can also download CAD files from us free of charge.
If a special part is essential, plastic plain bearings offer the greatest flexibility in component design due to their material specifications and modern manufacturing processes. Production using 3D printing, machining or injection moulding offers you great freedom in design.