Change Language :

For railway technology
With DIN EN 45545, the new material iglidur® RW250 fulfils the strict fire protection requirements of railway technology. In addition, the material formulation has been optimised for absolute wear resistance and offers very good running properties in many applications.

We have developed iglidur® RW250 for this purpose
The highest safety requirements apply to means of transport in local and long-distance public transport. One of these is the fire protection standard DIN EN 45545 for railway vehicles.
Bearings, which are used in the numerous mechanisms for seats, levers, flaps and doors, must fulfil these requirements in order not to endanger passengers in the event of a fire.
These - quite rightly - strict requirements pose major challenges for material development in bearing technology. In addition to the iglidur® RW370 bearing material already established in the industry, we have developed iglidur® RW250, an even more cost-effective material that is even more wear-resistant in the medium load range.

Online:
24h