Customer application examples

These customers are already reducing their costs with igubal spherical plain bearings

Solar tracker with tilted solar modules in a field.

By using our ESQM-120 pedestal bearing and the MLD sensor from DEGER in single-axis solar trackers, maximum light yield and a higher energy yield are achieved compared to rigid systems.

Single-axis solar tracker

igubal KBRM manus ornithopter with a detailed view of the drive mechanism.

The flying eagle V3 is so realistic that it can hardly be distinguished from a real eagle at a distance. With a wingspan of 190 cm and a wing beat frequency of around 2 to 3 Hz, it achieves a flight time of up to 26 minutes.

Ornithopter

Bronze artwork with two glass panels in front of red autumn trees.

The French company Arcora developed a system for moving sun protection slats on façades. The designers used plain bearings and spherical plain bearings from the igubal® series, among others.

Sun protection fins

A runner runs beside a stroller with a visible igus bearing symbol.

The JogAlong pushchair combines the usual transport function with sporting activity: it has ergonomically shaped arm levers that imitate the natural swing of the arms - making it ideal for combining running training with a walk for the child.

Jogging pram

A foiling catamaran sails with one person on board over choppy water.

The southern French shipyard Recreative Electric Vehicles is building an electric catamaran that is 80 per cent recyclable.

Catamaran

Formula Student race car from Arrabona Racing Team at sunset.

University students from the Arrabona Racing Team in Hungary are building a racing car that is designed to be particularly reliable and lightweight.

Race car

Field robot with display in a field, operated by a person in protective clothing.

Students at the French Institut Catholique Des Arts et Métiers have developed an automation solution for an agricultural machinery manufacturer.

Inspection trolley for seedlings

Sailboat with two people sailing in strong wind on rough seas.

The award-winning Seascape 24 sailing boat is a performance-orientated fast small cruiser that can also be used for leisurely cruising.

Seascape 24

ESQM bearing in a solar tracker for photovoltaic panels.

The company Axiom Research Labs in Bangalore has developed an automated modular single-axis solar tracker system (SPV system) for use on roofs and in solar parks.

Solar tracker

More about igubal spherical plain bearings

Shop

Tool

Knowledge base

Consulting

I look forward to answering your questions

visnevksi
Andrei Visnevski

Regional Manager for Baltics

+372 588 73933Write e-mail

Shipping and consultation