Change Language :

Automatic equalisation of parallelism errors,
1st floating bearing, 2nd fixed bearing
When using systems with two parallel guides, one side must be designed as a floating bearing. There is a suitable locating/non-locating bearing solution for every installation position, whether horizontal, vertical or lateral. This installation method prevents stiffness or jamming of the guide in the event of parallelism deviations between the guides. The floating bearing is realised by the controlled extension of the clearance in the direction of the anticipated parallelism error. This creates an additional degree of freedom on one side.
During installation, it is important to ensure that the floating bearing has approximately the same amount of clearance in both directions. The design of the fixed floating bearing system recommended by us can be seen in the illustrations below. The connection surfaces for the guides and carriages should have good evenness (e.g. milled surface) in order to avoid tension in the system. Minor unevenness in the connecting surfaces can be compensated to a certain extent by floating bearings.

floating bearing, selectable in all directions (+/- 1 mm), compensate for misalignment and parallelism.
Users can reduce installation work with the drylin® W square profile. floating bearings, which can be selected in all directions (+/1 mm), compensate for misalignment and parallelism between the rails. Jamming, which can otherwise only be prevented by time-consuming parallel alignment of the system, can be ruled out.
Although drylin® W is a profile rail system, angle errors around the x-axis can be compensated. An angle of +/- 7° is available for this purpose. This effectively eliminates the distortions known from the assembly of sheet metal parts.

The 2:1 rule,
1st floating bearing, 2nd fixed bearing
A few recommendations must be observed for the successful use of maintenance-free drylin® linear bearings**:** If the distance between the driving force and the fixed bearing is more than twice the bearing distance (2:1 rule), a static friction coefficient of 0.25 theoretically leads to jamming of the guidance.
The principle is not dependent on the load or the drive force. It is a product of friction and always relates to the locating bearing. The further away the drive is from the guide bearing, the greater the wear and the drive force required.
If the 2:1 rule is not observed when using linear plain bearings, the result is uneven movement or even blocking of the system. This can often be remedied with relatively simple modifications.
If you have any questions about the design and/or installation, please contact our application consultants.

Online:
24h