Change Language :

Temperature rating of +90°C: proven series, extended options
The servo and motor cable series CF270.UL.D, CF210.UL and CF21.UL as well as the CF 30 and CF 31 are now certified with a UL temperature rating of +90°C. This extends the application range of these series and provides additional safety for electrical application planning.
The standardisation of the 90° UL approval offers customers the opportunity to select the right cable from all the jacket materials on offer (PVC, PUR, TPE) and be sure that it will function safely in their mechanical energy chain application.
Calculate cable service life online

Online:
24h