Change Language :

The new simplicity of industrial intelligence.
There are technologies that improve an existing system.
And then there are technologies that connect two worlds at once – seamlessly, self-evidently, revolutionary.
With i.Cee², igus presents a module that does just that.
It is the next generation of the proven i.Cee system for superwise Gold and Platinum – and at the same time the first fully-fledged industrial PC from igus.
Developed for data logging, sensor technology, edge analytics and predictive maintenance in every conceivable system.
One device. Two tasks. Maximum effect.

i.Cee² continues the success story of the previous i.Cee module.
It takes over and extends all the core functions of the superwise services for e-chain systems:
In the superwise service levels Gold and Platinum, i.Cee² becomes the central nervous system of the entire
e-chain system.
It measures, understands and translates complex operating data into clear recommendations for action - in real time, reliably and based on data.
But this time the development does not end with monitoring.
It only begins there.

For the first time, an igus module goes far beyond the condition monitoring of energy chains.
i.Cee² is now also a fully-fledged industrial edge computer that can be integrated into completely new applications:
i.Cee² is therefore the first igus device that ranges from an e-chain system to a complete plant
- from a simple logger to an on-premise data centre in the control cabinet.
All this is included in the new i.Cee module:
| Technical data | |
|---|---|
| Equipment | Raspberry Pi CM4, Quad Core Cortex A72, 1.47″ TFT display, joystick for calibration diagnostics, 24 V supply, robust industrial housing. |
| System architecture | Docker/Kubernetes-compatible, REST MQTT APIs |
| Inputs and outputs | 12 digital outputs, 6 analogue inputs RS-485, 2 relay outputs, 2 load cell channels |
| Connectivity | 2x Ethernet (IT + fieldbus in parallel), WLAN, Bluetooth, integrated LTE modem, HDMI (for local visualisation), optional: LoRa |

Online:
24h