e-dispenser for shore-power supply

Save money and protect the environment

The visual shows a 3D animated representation of the energy supply of the e-dispenser: by using the energy chain, the cables are protected from sagging and damage as well as from impairment by UV radiation.

e-dispenser 2.0
Easy to use in existing systems

Tech up triangle

Tech up

Cost down triangle

Cost down

Proof square

Proof

Sustainability circle

Sustainability


How it works:

  1. Extending the energy chain:
    The energy chain is moved from the shore to the ship to establish the power connection.
  2. Power connection:
    The cables in the chain are connected to the ship via a junction box and connector.
  3. Stable supply:
    While the ship is in port, the chain remains in position and reliably supplies it with shore power.
  4. Return:
    After depositing, the energy chain is retracted automatically or manually.
Cross-section diagram of a 3 x 95 mm² multicore cable with an outer diameter of 70mm

Multi-core cable with 3 x 95²

Illustration of a cross-section diagram of an igus energy chain TRC.125.182.0 with filling. The filling consists of three 95mm² CFCRANE.PUR cables. By using this cable, which was designed for demanding applications, the bend radius could be reduced to 300mm.

3 x chainflex CFCRANE.PUR (95²) + triflex R TRC.125.182.0


4-year guarantee - complete peace of mind!

The icon - an 8 with "Long life" on the top and "guaranteed" on the bottom, with an orange arrow rising from the bottom to the top inside it (similar to an upside-down hourglass). The icon visualises the guarantee promise of the company igus.
  • Conveyor unit with triflex R energy chain, chainflex cables, connectors, junction box, harnessing - everything tested and with a 4-year guarantee.
  • With this, we offer a standard energy supply unit that is individually adapted to the situation on site and the respective customer requirements, developed and constructed as a complete solution.
  • Also for other industries, e.g. mechanical engineering, robotics and welding applications, the e-dispenser module represents an interesting energy supply solution. In all cases, users benefit from standardised (and hence tried, tested, and cost-effective) energy supply components.

More information

The visual shows a container ship at the quay. Two thick red cables are currently being lowered for shore power supply.

Further products for shore-power supply

The image shows a round energy chain - the triflex R. It is used especially in robotics and is offered in various sizes and designs

triflex R

The image shows a black energy chain. At the right end of the chain, different round cables can be seen with the respective connectors. The logo with the inscription "guarantee", "igus products" and "4 years" can be seen on the chain. This statement clarifies that igus also grants a 4-year guarantee on its harnessed solutions - the readychain - provided that the technical conditions are met.

readychain harnessing

Consulting

I look forward to answering your questions

visnevksi
Andrei Visnevski

Regional Manager for Baltics

+372 588 73933Write e-mail

Shipping and consultation