Change Language :

The new igus® standard for support plates and floating moving ends with identical hole pattern and the same attachment height for an even more installation-friendly connection of the e-chain system® to the moving end. The system is supplied with an integrated holder for the strain relief. The i.Sense EC.P push/pull force monitoring system can be ordered as an option or retrofitted at a later date. This significantly reduces downtime costs and continuously increases overall system effectiveness.
Note: The parts supplied are NOT the transparent ones. Energy chain, cables and trough system are not part of the offer.

Online:
24h