Change Language :

Our tried and tested iglidur standard materials are now all available without PTFE. New additions are iglidur GPF, HPF and XPF, which extend our PTFE-free range by one material for universal use, one for high temperature and one for chemical contact.
100% comparable or better wear properties compared to PTFE-based solutions
Only 10% more expensive than PTFE-based solutions
Proven in over 15,000 wear tests in the industry's largest test laboratory
Sustainable due to the absence of PTFE or forever chemicals
igus supports the circular economy of plastics and invests in chemical recycling. Find out more.

Magnus, as Head of Materials Development: How far along is igus with the topic of PFAS and PTFE?
We are continuing to develop PTFE-free alternatives to our most successful PTFE-containing materials at full speed. The main focus here is on expanding our top 5 plain bearing materials to include variants without the fluorine additive. The aim is to develop PTFE-free variants with the same or better specifications than the originals that contain PTFE. In 2024, we already presented the iglidur JPF and iglidur WPF materials. These are PTFE-free versions of the highly versatile and proven iglidur J, as well as the iglidur W300, which is optimised primarily for somewhat higher loads and wear requirements. We have also developed a recipe for a PTFE-free iglidur F. Now, just in time for Hannover Messe 2025, we can announce a major breakthrough. We have made PTFE-free versions of the most successful iglidur material – iglidur G - and we can now also offer the high-temperature standard iglidur X as PTFE-free. With iglidur HPF, we also offer a variant especially for use in liquid media.
The white paper "Focussing on PFAS: planned restrictions, challenges and solutions for the industry" deals with the following topics, among others:

You can find more PTFE-free plain bearing products in our online shop.


Online:
24h