Change Language :

iglidur® M210 - highly wear-resistant in the medium load range
The new iglidur® M210 was specially developed for use in the medium load range with swivelling loads. In addition, care was taken during development to ensure that the material can be used particularly well for injection-moulded thick-walled bearings. This makes iglidur® M210 particularly suitable for applications in which thick-walled bushings are to be used or replaced that are also as robust as possible.

We have developed the iglidur® M210 for this purpose
In practice, particularly thick-walled plastic plain bearings actually offer hardly any advantages over thin-walled ones. Nevertheless, thick-walled bearings are often required, especially when replacing metal bearings with plastic ones. Once designed in, it is often time-consuming to use other bearing dimensions.
This is why we offer iglidur® M210, a new bearing material especially for use as a thick-walled plain bearing. The material also offers particularly good wear properties for medium loads up to 50 MPa surface pressure in swivelling applications.

Online:
24h