Change Language :

Particularly suitable for e-coated assemblies and highly wear-resistant.
The new iglidur F300 material was primarily optimised for requirements that occur before the actual application as a plain bearing. Particularly in the production of automobiles, but also for other vehicles or furniture, already partially assembled assemblies are provided with a cathodic dip painting (e-coating). In this process, the assembly is placed under electrical voltage, immersed in aqueous paint and then dried at high temperatures.
This process places special demands on the stability of the material and only works if it is sufficiently electrically conductive. iglidur F300 offers very good conductivity for plastics. It also offers mechanical and thermal stability and good durability.
What we developed iglidur F300 for
The e-coating process places special demands on plain bearing materials. They must be conductive because the paint can only adhere to those areas that are electrically charged. In addition, high temperatures are generated during drying, which can impair the mechanical stability of many plastics.
Optimised specifically for these requirements, the new plain bearing material iglidur F300 is ideal for applications in which pre-assembled components with pressed-fitted plain bearings are e-coated. These include applications in automobiles and commercial vehicles, but also in furniture or bicycles.
Due to the current discussion about a ban on PTFE or PFAS, we have compiled all the important information relating to our plain bearings here. You will also find a list of all iglidur materials that do not contain PTFE or have been tested for PFAS which are known to be harmful to health.

Online:
24h