Change Language :

The new material iglidur A351 is ideal for use in applications with food contact that operate at high temperatures in corrosive environments.
Resistant to wear and media at high temperatures
Up to 75% more cost-effective than PEEK-based alternatives, with a service life that is up to three times longer
Tested in the igus® tribo laboratory (rotating wear: 0.3m/s, 2MPa, 304 stainless steel; A351: 11.52μm/km, PEEK: 41.2μm/km)
In view of the current discussion about a ban on PTFE or PFAS, we have put together all the important information about our plain bearings here. In addition, you will find a list of all iglidur materials that do not contain PTFE or that have been tested for PFAS that are considered critical or harmful to health.


Online:
24h