Change Language :
Transmitting data volumes quickly and without interference
The technical requirements for energy supply systems in mechanical and plant engineering demand functionally reliable cables. igus® The company , Cologne, is increasingly relying on glass fibre optic cables, which allow very high data volumes with increasing cable lengths. The "chainflex® CFLG.2HG" product family is now available as sold by the metre or assembled with connectors from stock.

Fibre optic cable endurance test in the igus®® laboratory: 60,000 kilometres covered in the energy chain without interference.
The glass fibre optic cable of the CFLG.2HG series was also tested for two years in the igus®® energy chain laboratory. A travel of 2 m with a bend radius of only 100 mm and a speed of 2.5 m/s was selected. Even after more than 30 million movements in the energy chain - that is 60,000 kilometres - no technically relevant increases in attenuation were detected. The end of the test is not yet in sight.
Here you can find the products used
You can find more interesting applications from a wide range of areas here

Online:
24h