Change Language :


The bend radius describes the radius in which a cable can be bent without damage. The key factor is the so-called neutral axis, meaning that the cable is positioned centrally within the chain.
Basic rule:
The smaller the bend radius, the higher the material quality must be and the individual cores must have an appropriate stranding design.
A simple example:
As in the human body, the stronger the bend, the greater the load. Exceeding the maximum permissible bending capability may result in damage.
Why is the right bend radius so important?
Incorrect selection of bend radii can have significant consequences:
In practice, there are different applications:
In energy chains, the ideal bend radius depends on the cable with the largest outer diameter.
Important rules:
The minimum bend radius is the permissible smallest bend radius, below which a cable must not be bent.
The ambient conditions play a central role:
At low temperatures:
At high temperatures:
Bending below the minimum bend radius often leads to premature failure.

A frequently used simple rule is:
Minimum bend radius = 10 × cable diameter
Example:
A cable with a diameter of 10mm → Minimum bend radius = 100mm
Note:
This value can vary depending on application, material and standard.
Never fall below the manufacturer's specifications
Choose the largest possible radius
Take into account the application (static vs. dynamic)
Take temperature conditions into account
Use special cables for tight radii
Guide cables neatly and provide proper strain relief
With very tight bend radii (e.g. < 5x diameter), conventional copper cables reach their physical limits.
The areas of application for cables with tight bend radii are diverse. They are particularly needed in applications where flexible and dynamic movements must be carried out in the smallest possible installation space. For example, they are used in the semiconductor and assembly industry, mechanical engineering, and the automotive sector. New application possibilities arise in automatic doors for vehicles and trains as well as in automatic self-service food vending machines and the packaging industry.
Cables with small bend radii
Dynamic applications with tight bend radii quickly cause the copper cores of conventional cables to meet their mechanical stress limits. Especially in areas of application that only have a small installation space but require a high number of strokes, special igus cables offer increased operational safety.
In addition to cables with conventional copper strands with a very short pitch length, igus also offers alloy conductors that can achieve bend radii of up to 3xd. In addition, cable jacket materials with exceptionally high abrasion resistance and flexural durability are used. With its many years of experience in its own test laboratory, igus can guarantee a long service life and planning reliability for chainflex cables with the smallest bend radii in energy chains.
Only up to the specified minimum bend radius. Exceeding this value can lead to damage.
This leads to material fatigue, cable breakage, or malfunctions.
Yes, among others, IEEE, ICEA and DIN specify guide values.
The maximum possible radius within the structural constraints.
Yes, extreme temperatures affect the flexibility and thus the permissible radius.

Online:
24h