Change Language :

Our Smartfit laser metre is a helpful tool for bicycle retailers. It consists of an igus NSV-01-27 rail with a laser-engraved scale and prism carriage paired with a cross laser. The laser metre is ideal for making precise measurements and settings on the bike. This allows salespeople to determine the optimum frame height and end customers to go on a test ride with perfect adjustments. Our distributors also use it for the individual final assembly of bicycles before delivery. It impresses with its high-precision, easy handling ... Important requirements are: the laser metre and the corresponding rail guide must be robust so as to prevent them from going to rack and ruin in everyday business. The system must be easy to operate and be able to "keep" the set values. An additional challenge, which is relevant for our customers, is the price-performance ratio ... We particularly appreciate the lubrication-free pre-load prism slide, which has proven its worth in working environments such as bike shops and workshops.

Online:
24h