Change Language :

X = load [MPa]
Y = wear [μm/km]
Wear of iglidur plain bearings at low loads, shaft: Cf53, v = 0.1m/s
As the wear of components depends on many different factors, it is difficult to make general statements about the wear behaviour. In a wide range of experiments and tests, measuring wear is the main focus. In testing, it has become clear what deviations are possible between different material pairings. At given loads and surface speeds, wear resistance between common material pairings can still vary slightly by a factor of 10.

X = load [MPa]
Y = wear [μm/km]
Wear of iglidur® plain bearings at medium and high loads, shaft: Cf53, v = 0.1 m/s
Different loads greatly influence the bearing wear. Among the iglidur plain bearings, certain materials are optimised for low loads while others are suitable for use with high or extremely high loads. With its hardened, ground shafts, iglidur J can be described as the most wear-resistant bearing material for light loads. iglidur Q, in contrast, is the specialist for extremely high loads.
Within wide temperature ranges, the wear resistance of iglidur plain bearings changes only slightly. In the upper temperature range, however, the influence of the temperature increases, and the wear of the plain bearings intensifies disproportionately.
The table below compares the so-called wear limits.
Iglidur X is a special exception in this respect. The wear resistance of iglidur X plain bearings at first increases significantly and reaches its optimum at a temperature of +160°C. Then resistance decreases again, gradually.
Have you not found the required material? There is extensive data on all materials and data sheets in our online shop.
| Material | Temp. [°C] |
|---|---|
| iglidur G | +120 |
| iglidur J | +70 |
| iglidur M250 | +80 |
| iglidur W300 | +120 |
| iglidur X | +210 |
| iglidur K | +90 |
| iglidur P | +100 |
| iglidur GLW | +100 |
| iglidur J260 | +80 |
| iglidur J3 | +70 |
| iglidur J350 | +140 |
| iglidur L250 | +120 |
| iglidur R | +70 |
| iglidur J200 | +70 |
| iglidur D | +70 |
| iglidur V400 | +130 |
| iglidur X6 | +210 |
| iglidur Z | +200 |
| iglidur® UW500 | +190 |
| iglidur H | +120 |
| iglidur H1 | +170 |
| iglidur H370 | +150 |
| iglidur H2 | +120 |
| iglidur A180 | +70 |
| iglidur A200 | +80 |
| iglidur A351 | +120 |
| iglidur A500 | +190 |
| iglidur A290 | +120 |
| iglidur T220 | +90 |
| iglidur F | +130 |
| iglidur H4 | +120 |
| iglidur Q | +80 |
| iglidur UW | +70 |
| iglidur B | +70 |
| iglidur C | +70 |

Online:
24h