Change Language :
Material table
General specification
Unit
iglidur® D
Test method
density
g/cm³
1,40
Colour
green colour
max. Moisture absorption at 23°C/50% room humidity.
% by weight
0,3
DIN 53495
max. total moisture absorption
wt.-%
1,1
Sliding friction coefficient, dynamic, against steel
µ
0,08 - 0,26
pv value, max. (dry)
MPa x m/s
0,27
Mechanical specification
flexural modulus
MPa
2.000
DIN 53457
flexural strength at 20°C
MPa
72
DIN 53452
Compressive strength
MPa
70
maximum recommended surface pressure (20°C)
MPa
23
Shore D hardness
78
DIN 53505
Physical and thermal specification
Upper long-term application temperature
°C
+90
upper short-term application temperature
°C
+110
Lower application temperature
°C
-50
thermal conductivity
W/m x K
0,25
ASTM C 177
coefficient of thermal expansion (at 23°C)
K-1 x 10-5
11
DIN 53752
Electrical specification
Volume resistivity
Ωcm
> 1014
DIN IEC 93
surface resistance
Ω
> 1014
DIN 53482
Table 01: Material data

diagram. 01: Permissible pv value for iglidur® D plain bearings with 1 mm wall thickness in dry operation against a steel shaft, at +20 °C, installed in a steel housing
X = surface speed [m/s]
Y = load [MPa]
When developing iglidur® D as a plain bearing material, a very low price was at the top of the requirements profile. In addition, low coefficients of friction were to be achieved in dry operation, especially at high speeds. The silicone-containing material also achieves outstandingly low friction values in dry operation and runs largely stick-slip-free.

diagram. 02: maximum recommended surface pressure as a function of temperature (23 MPa at +20 °C)
X = temperature [°C]
Y = load [MPa]
Mechanical specification
The maximum recommended surface pressure is a mechanical material parameter. It cannot be used to draw conclusions about tribology. The compressive strength of iglidur® D plain bearings decreases with increasing temperatures. diagram. 02 illustrates this relationship.

Diagram 03: Deformation under pressure and temperature
X = load [MPa]
Y = Deformation [%]
iglidur® D bearings were mainly developed for low radial loads. diagram.03 shows the elastic deformation of iglidur® D under radial load. Under the maximum recommended surface pressure of 23 MPa, the deformation is approx. 3%. Plastic deformation can be neglected up to this value. However, it also depends on the duration of the impact.

Diagram 04: Coefficient of friction as a function of the surface speed, p = 0.75MPa
X = surface speed [m/s]
Y = coefficient of friction μ
Friction and wear
The coefficient of friction decreases in the same way as the wear resistance of the load to be carried. The coefficient of friction reaches its optimum in the Ra range between 0.4 and 0.6 μm.

Diagram 05: Coefficient of friction as a function of the pressure, v = 0.01m/s
X = coefficient of friction μ
Y = load [MPa]
iglidur® D
Dry
Fat
oil
water
coefficient of friction µ
0,08 - 0,26
0,09
0,04
0,04
Table 04: coefficient of friction against steel
(Ra = 1 µm, 50 HRC)

diagram. 06: Wear, rotating application with different shaft materials, p = 1 MPa, v = 0.3 m/s
X = Shaft material
Y = wear [μm/km]
A = aluminium, hard anodised
B = free cutting steel
C = Cf53
D = Cf53, hard chrome-plated
E = HR carbon steel
F = 304 SS
G = high grade steel
Shaft materials
Diagrams 06 and 07 show an extension of the results of tests with different shaft materials that were carried out with plain bearings from iglidur® D.
If your intended shaft material is not included in this list, please contact us.

Online:
24h