Change Language :
An igubal® spherical ball has been integrated into the swashplate of a reverse birotor drone. The special feature of the "FSS3 Drone" is that it is controlled by two helicopter rotors and the swashplate is attached directly to the mast. All components have to function at different temperatures, humidity and under heavy loads. The assembly of the spherical ball is innovative for several reasons: it is optimised for the weight level and uses only one component.
Civic Drone, Antoine Praquin, Montesson, France

Online:
24h