Change Language :
Shore power, also known as cold ironing, is an environmentally friendly solution for supplying ships in port with power without having to rely on their diesel-powered generators. This reduces emissions and noise and allows ships to keep their main engines switched off while still receiving power for lighting, air conditioning and other systems. We at igus help simplify shore power supply and enable efficient and practical connection of ships to the power grid, regardless of where they are berthed in the port.
Many people may already be familiar with shore power, but under a different name. For this reason, here are some of the most common synonyms for shore power:
In order to gain a better insight into the topic of shore power, it is helpful to know and familiarise yourself with some key terms:

Every port is unique. Tidal behaviour, terminal designs and equipment differ from one port to another. Ships equipped for shore power supply have a cable drum on board that allows two cables with connectors to be lowered onto the quay. These can then be connected to sockets on the quay. There are three conditions for finding the optimum location for a fixed socket:
1. Difference between ships' shore power locations
2. Onboard CMS constraints
3. Berth arrangement flexibility
The self-propelled iMSPO system from igus offers the solution. It is able to provide a shore-side power outlet for the ship's cables wherever they are needed along the berth at a distance of 400m and more.
The maritime industry is at a turning point when it comes to reducing its environmental impact and promoting more sustainable practices. One key technology helping to drive this transformation is the igus shore power solution. At igus, we are at the forefront of developing innovative systems that enable ships to switch to clean energy sources when docked. Our systems include the following:
One of the biggest advantages of shore power is the drastic reduction in harmful emissions. Ships that switch to shore power when docked in port can switch off their diesel generators, which leads to a significant reduction in nitrogen oxides, sulphur oxides, particulate matter and carbon dioxide. These emission reductions are not only good for the planet, but also for the health of people who live near ports.
With fewer ship emissions, air quality improves in and around port areas. This is particularly important for cities where the port is an integral part of urban life. Cleaner air means fewer respiratory illnesses and a higher quality of life for local residents and port workers.
Shore power also contributes to a quieter environment, as the ship's engines and generators can be switched off. This reduction in noise is not only pleasant for the ears, but also promotes a stress-free environment.
Shore power is often more efficient than power generation on board ships. When this power comes from renewable sources, efficiency is increased even further, leading to an even greater reduction in the carbon footprint.
By using shore power, ships can reduce their consumption of fossil fuels. This not only helps reduce pollution but also lowers operating costs for shipping companies.
igus shore power systems are an essential component of green port initiatives that aim to minimise the environmental impact of shipping traffic. They demonstrate the commitment of port authorities and shipping companies to make the maritime industry more environmentally friendly.
The implementation of igus shore power systems is a clear sign that the maritime industry is ready to invest in sustainable technologies. This not only promotes environmental compatibility but also strengthens the industry's image as responsible and future-oriented.
Various requirements and standards must be met in order to install shore power both in a port and on board ships. Both the port and the ships themselves are affected.
At a time when sustainability and environmental protection are becoming increasingly important, the use of shore power offers considerable economic benefits for port operators and shipping companies. From 2030 onwards, every port in Europe must have a shore power supply system. Act early with igus rather than too late. The following points are a plus for every port and can be achieved with solutions from igus:
As of 2030, the use of shore power will be compulsory throughout the EU for container and cruise ships with a gross tonnage of over 5,000. From this point on, any combustion processes at the quayside will also be prohibited. Port of Hamburg | Shore power for ships)
igus® is characterised by the provision of innovative, durable and flexible solutions. The igus® iMSPO can be moved along the quay, which improves connection options for ships. We also rely on our high-quality chainflex® cables and e-chain® energy chains, which are known for their durability and reliability.
Installation time can vary depending on the complexity of the project and the specific requirements of the port. With all the necessary permits and preparations, installation can typically be completed within a few weeks.
Contact us for a detailed assessment tailored to your needs.
The costs for an igus® Mobile Shore Power Outlet (iMSPO) depend on the specific requirements of the respective port and the length of the quay. For an exact price quotation, we recommend contacting us directly to receive a customised solution.
Ports that do not comply with the EU emission reduction regulations by 2030 could face penalties and trade restrictions. This can have a negative impact on the profitability and growth of the regions concerned.
The power we provide can be compared with that of the original diesel engines, but with the advantage of a significant reduction in emissions.
We have already worked with various ports worldwide to implement shore power solutions. Examples include the Port of Hamburg, which is expanding its shore power infrastructure, and a floating LNG storage terminal in Bahrain, which is equipped with an igus® solution.
Shore power has developed significantly over the years and is now an indispensable part of modern port infrastructure. Originally known as
"cold ironing", the technology has developed from early coal-fired engines to today's state-of-the-art electrical systems.
Origins during the Second World War
Ships such as the USS Wiseman served as mobile power stations during World War II, supplying power to towns and ports. These early applications of ship energy sources on land were not identical to today's shore power, but they laid the foundation for the idea of connecting ships to shore power.

Start of shore power connections
In the 1980s some ports, especially in environmentally conscious regions, took their first steps towards implementing shore power, mainly for smaller vessels. These early initiatives were often pilot projects aimed at demonstrating the feasibility and benefits of the technology.
Growing environmental awareness
The first discussions on reducing emissions in port cities led to more attention being paid to shore power. It was recognised that the use of shore power could significantly improve air quality in the ports. As a result, the first major implementations of shore power have been carried out in some ports.
Regulatory developments
In the 2000s, stricter environmental regulations in many countries led to increased investment in shore power systems by ports and shipping companies. California was one of the pioneers, introducing regulations in 2007 that prescribed the use of shore power for certain types of ships.
Development of shore power connection in recent decades
In recent decades, many ports worldwide, including the Port of Hamburg, have significantly expanded their infrastructure for connecting shore power. These developments are part of global efforts to reduce emissions and improve air quality in port cities. We at igus® are proud to be part of this development and to offer innovative solutions that meet the demands of modern shipping.
The future of shore power
The future of shore power looks promising. With continuous improvement in technology and increasing acceptance worldwide, more and more ports and ships are expected to switch to this environmentally friendly solution.
This is particularly true given that from 2030, all container ships and passenger ships in major EU ports must use shore power.
Connection solutions - offshore and LNG terminals
Offshore terminals and ships place high demands on the flexibility and reliability of energy chain solutions, especially in combination with extreme weather conditions and changing berthing positions. LNG terminals require robust and low-maintenance shore power solutions that can cope with the challenges of long distances, harsh environmental conditions and constant operational readiness, for which the OSC energy supply system is ideal. Both areas need systems that can compensate for movements due to tides, wind and waves and implement emergency mechanisms. Such a system can also be found in our user report on the FSU in Bahrain.

We test our shore power systems for you under real conditions and in all weather conditions in our in-house test laboratory. Around a third of our 5,000m² test laboratory for every industry is located in the outdoor area at the igus headquarters in Cologne. This is where our energy chain systems for onshore power supply and offshore applications are tested for their suitability in wind and weather - both on long travels and vertically on test towers.

Online:
24h