Change Language :
Energy safely guided - in all directions and with small bend radius
Welding and gluing robots are a key component in the automated production of electric and hydrogen drives. These precise machines are characterised by high manoeuvrability and speeds. In order to keep up with this, the individual components installed must also fulfil certain requirements. Energy chains, which are assembled on the outside of the robot, should be movable but at the same time reliably protect the cables and material hoses even with a small bend radius. The energy chain should also be easy to open so that cables or media hoses can be replaced quickly.

Our service starts even before installation:

Online:
24h