Change Language :
You can realise many different areas of application with robots. For example, in addition to positioning and pick-and-place tasks, it is also possible to efficiently automate the packaging of products. Our robot systems insert your components precisely and with consistent quality. The processes are exactly repeatable. Another reason is workplace safety; the robot can work in a wide variety of environments without any problems and provides support for non-ergonomic work. Thanks to the user-friendly set-up and control system of the robot, as well as the modular principle of our robotic components, the packaging applications can also be flexibly customised. Our Low Cost Automationexperts will be happy to support you in the realisation and selection of your complete robot system.
The automatic labelling machine for Beindlhof farmhouse ice cream automatically closes and labels the tubs. The system has to differentiate between 200 flavours during operation and apply the labels accordingly.
Every week, four machines with around 20 employees produce around 100,000 surgical and FFP2 masks. Two fully automatic packaging systems are used for the manual and monotonous packaging of the masks. This increases production times and reduces unit costs.
A linear drive from igus® is used for the 3D camera, which is used in the packaging of furniture and is mounted at a height of 3 metres. By using the linear axis in combination with the camera, a complete image processing system can be dispensed with, as the camera is moved to the respective position.

Online:
24h