Change Language :
RWE Power AG uses igus chainflex as a standard cable for bus systems
The heavy load to which electrical cables are subjected in open-cast lignite mining becomes immediately clear when you watch one of the mighty bucket-wheel excavators at work in the Rhineland mining areas. The operator of the open-cast mines, RWE Power AG, decided to include igus chainflex cables in the factory standard after extensive tests. Customised, optimised cables are used that are especially resistant to mechanical stress.
From the point of view of the cable specialists, it is interesting that the main characteristic of the chainflex types - their chain suitability - is not even needed in most cases. The focus is more on typical heavy-duty specifications such as abrasion resistance and UV resistance. However, there are exceptions. In June/July 2013, one of the seven bucket-wheel excavators built in the 1970s underwent major maintenance. In the course of this work, the slip ring assembly in the powerful slewing ring of the excavator was replaced with a large, approximately one metre wide igus energy chain, which is of course also filled with the newly standardised bus cables.
RWE project engineer Jürgen Lenz: "The energy chain saves space and is less susceptible to wear. We also incorporate additional features, such as a water supply system to operate the dust control equipment on the bucket wheel and conveyor line of the large-scale machinery, which helps us prevent dust from forming during mining operations." The wide range of other cables for the energy chain enables a total solution of all cables for this application. Starting from the described bus cables up to medium voltage cables. The trough and lining were installed by igus employees, who also took care of the assembly of the cables and the filling. In order to create access to the assembly site, a narrow access hatch first had to be cut through the thick steel structure at the connection between the crawler track and the superstructure.

Online:
24h