Change Language :

The UniShed 2 developed by Gitec GmbH is the world's first harnessless Jacquard weaving machine.
With the UniShed2, Gitec GmbH has developed a completely new type of weaving machine and therefore a real innovation. This is because the machines work without the electromechanical "harness" and instead utilise vibrating axles, which are supported in plain bearings from igus®. Bearing bushes made from the high-performance polymer iglidur® J3 are used.
The textile industry is closely associated with the name Jacquard: Around 1800, Joseph-Marie Jacquard invented the loom named after him in Lyon, which scans the individual weaving pattern via punched cards. He thus made an important contribution to factory automation and also to the development of computer technology: almost a hundred years later, pioneers such as Herman Hollerith used punched cards as data carriers for the first machines for automated data acquisition.
"We initially used plain bearings from another manufacturer, which worked perfectly technically but were quite expensive. As the textile industry is very price-sensitive and each individual axis is stored many times, we switched to igus® bearings."
Roland Micheln, Head of Development at Gitec GmbH

igus sales consultant Joachim Mayr and head of development at Gitec Roland Michel
This innovation offers numerous advantages. Head of Development Roland Michel "The machines allow absolute freedom in patterning because the process can be better controlled. They work extremely reliably because every single thread is monitored optically. The machines are also very compact and consume around 20 per cent less energy."
A first prototype of the UniShed 2 is already being field-tested by a user and others are being trialled at Gitec. The development is attracting a great deal of attention in the textile industry and Gitec expects sustainable market success: "We are convinced that the new principle will replace the old technology by 80 per cent."
In addition, the moisture absorption of this material, which has been included in the standard programme along with 15 other high-performance polymers since the beginning of the year, is lower. This specification is also very important for Gitec, as Roland Michel explains: "Our machines are often used in countries where the humidity is very high. There, the plastic can swell during storage, which affects the bearing clearance."

Online:
24h