Change Language :

control cable for narrowest bend radius ensures operational safety in low-floor trains
Public transport must be safe under all circumstances. There must be no disruption to operational processes. The doors are often the centre of attention. In this example, a cable used in a moving energy supply system ensures smooth opening and closing. Improved conductors and sheath materials ensure that there are no more failures despite high continuous loads.
The control cable is primarily responsible for the monitored opening and closing of the doors. It is a safety-relevant part that requires a great deal of attention during all inspections. "To keep our costs as low as possible, we endeavour to only replace wear-resistant parts with high-quality components that meet the latest state of the art," explains Ernst Baerhausen. "And the longer the service life of the cable, for example, the longer the maintenance intervals and therefore our economic costs are reduced," adds Hans Bennerscheid.
"The main difference to comparable cables lies in the conductor," explains Rainer Rössel, Head of Development and Marketing for chainflex® and readychain® at igus®, in conversation. "Copper ages and becomes brittle over time. The CF98 cable is no longer pure copper, but a special alloy that is designed for considerably higher mechanical stress."
It has only a slightly lower conductivity compared to pure copper, which was compensated for with a slightly increased cross section - approximately 10 % larger outer diameter compared to a comparable type. However, in view of the considerable increase in requirements in recent years, it is certain that such high-quality solutions will be needed more and more frequently in order to guarantee operational reliability in the critical area of the very small cross section. It makes new applications in energy supply systems possible - for example in the automation sector, in the packaging industry, in the assembly and semiconductor industry as well as in the automotive and banking sectors.
Cable for all cases
"Although we come from the mechanical and plant engineering sector, our cables can demonstrate their strengths in many safety-relevant parts such as automatic doors in buses and trains," explains Rainer Rössel. "In the public transport sector in particular, for example, we have been able to realise solutions to problems with very high train loads in some cases, which ultimately led to greater passenger safety, higher operational readiness and therefore greater cost-effectiveness." Many railway doors have already been equipped with our cables to ensure significantly higher functional reliability. As there is no minimum quantity purchase or surcharge, follow-up costs are also reduced. Over 750 cable types can be supplied from stock worldwide.
Here you can find the products used
You can find more interesting applications from a wide range of areas here

Online:
24h