Change Language :
Single-core cables from igus® are used in the high-performance turning centres from EMAG
The vertical EMAG turning centres of the VMC series are also available as "five-axis machines", which allow the machining of complex geometries. For example, they can be used to machine angled holes and surfaces in heavy components. This is a challenge for the power supply of the spindle. EMAG relies on single-core cables from the chainflex® programme from igus®.
"If a motor cable fails and needs to be replaced, this means a day of downtime due to the very compact design. That's why a high-quality and resilient spindle cable is an important design feature."
Markus Pannicke, Lead Engineer Cables and Conductors at EMAG Leipzig
Thanks to over 25 years of practical experience and countless tests in the 3,800 m² test laboratory in Cologne, igus® has been the only manufacturer on the market to offer a guarantee of 36 months, or up to 40 million double strokes, on its chainflex® cable range for over five years. The online service life calculator can also be used to determine the expected service life of the chainflex® cable beyond the warranty period. In EMAG's case, the solution with the CF270.UL.D spindle cable means a high saving in installation space and a simultaneous reduction in costs. Thanks to the comprehensive and resilient guarantee from igus®, there is no risk for EMAG.

Online:
24h