Change Language :

Motorised mirrored ceiling
Installation of 120 mirrors
The TWAXIS mirror installation was developed by MACHINESHOP to create a unique decoration for the advanced cruise fleet of MSC Cruises. An extraordinary, motorised mirrored ceiling was created, which can be admired by passengers three storeys up.
MSC Cruises is known for its ultra-modern ships with a sleek, modern design. Therefore, this project required a matching, elegant solution with high reliability. MACHINESHOP developed a ceiling structure consisting of 120 mosaic-like, pentagonal mirrors that move almost silently. Programming makes it possible for the mirrors to move in different patterns. This makes it look as if the ship's ceiling is breathing or dancing.
You can find more information about MACHINESHOP here: www.machineshop.co.uk
You can find more information about the TWAXIS project here: www.twaxis.com
Special parts tailored to the application were used for the project. Here you can see the standard products on which these special parts are based.

Online:
24h