Change Language :
A normal truck was converted into a food truck by Nomes srl.Various products can be offered there such as pizza, hamburgers, ice cream and much more. Sliding and hanging cabinets for selling goods are installed on the ceiling of the vehicle. The drylin N linear system allows the elements to be adjusted variably. Moving a cabinet element to the rear position ensures a perfect view of the rear-view mirror and side window for the driver of the vehicle. The adjustment in the front position, on the other hand, allows the coverage of the driving area during sales times and a significant increase in the display area for the products offered for sale.
Functional stowage and storage shelving, attached at the top to drylin N low-profile guide system.
This allows the shelving to be moved smoothly.
It is designed for the efficient utilisation of the limited space.

Online:
24h