Change Language :
At the Eschweiler waste incineration plant, we replaced the existing trailing cables with an energy chain that was developed from the ground up for use under adverse environmental conditions. The installation of the chain on the 70 metre long crane runway placed high demands on logistics and coordination because it was carried out while the incineration lines were in operation.
"In general, the energy chain on the crane runway is much more accessible than the trailing cable. We can carry out maintenance work without the need for an additional platform. In addition, the elimination of the trailing cable creates additional space for the walkway along the crane runway, so that the entire crane maintenance is now easier."
Wolfgang Krebs, Electrical and Control Technology Manager at RWE Power AG

Online:
24h