Change Language :
A P4.1 series roller energy chain is in operation at the Port of Rotterdam, one of the largest bulk handling ports in Western Europe. On the huge ship-to-shore crane, it operates without incident despite 24/7 continuous operation and a travel distance of over 100 metres. So far it has completed more than 9,000 operating hours.
Download the case study
This case study clearly describes how EMO B.V. was able to achieve running performances of over 375,000km on its STS cranes with igus chains for cranes®.


Online:
24h