Change Language :
For the guidance of cables on passenger boarding bridges, the gangways, e-chain® are used here, which are telescopically moved one above the other under the passenger boarding bridge. They replace previous festooning systems, which have proven to be unreliable. The e-chain® are laid out on their side, so that the system can also be designed more compactly and looks even better, as there are no more cables hanging down from the gangway.
JBT Aerotech, Herb Mudrow, Ogden, Utah, USA

Online:
24h