Change Language :
"FitoStinger" is a drone for pest control: an extendable arm can be brought very close to the infested area to spray a pesticide, for example. A drylin® linear guidance system is used to move the arm. igubal® bearings are used in the guide system of the transport tubes containing the pesticide and in the articulated arm. An energy chain from the E2 micro series is also used. The materials used have the required strength and rigidity for this application and are also extremely light.
TSA CENTER / ADRONELINE, Iván, Sanz Martínez, Cerdanyola del Valles, Spain

Online:
24h