Change Language :
motion plastics are high-performance plastics that are used throughout industry – and do not require lubrication after installation.
This means not only savings on expensive lubricating greases and oils.
Customers also save on maintenance time, personnel costs, the risk of incorrect or insufficient lubrication, system downtime and harmful substances that end up in the environment or in the drain. We call this: "GO ZERO"

This saves Lemken 22 lubrication points per cultivator.
This saves Huppenkothen 220 maintenance cycles per mini excavator.
This enables Heineken Brazil to save up to 28 tonnes of CO2 equivalent per year.

In this white paper, we show which industries and companies are already successfully using lubrication-free and maintenance-free bearing technology and how much they benefit from the cost savings.
Finding a spot on this list are Heineken Brasil (beverage technology), KettenWulf (drive and conveyor technology) and Rockinger (agricultural engineering).
Other topics:

... specialises in the manufacture of agricultural equipment. This includes the Karat 9, an intensive cultivator with tines up to 30 centimetres long. To prevent damage to the tool, the tines deflect when subjected to excessive force, such as from stones in the ground.
To ensure the deflection movement, metal bearings were used on all tines. However, the metal bearings had to be lubricated for up to an hour every day. Failure to do so would have led to corrosion and wear.
The iglidur bearings used today operate completely without external lubrication, as the material contains self-lubricating solid lubricants. This not only saves the farmer time later on, but he also benefits from the high load-bearing capacity of the bearings, their lower susceptibility to dirt and the increased service life of the plain bearings.
Lubricant cost saved
Personnel costs saved
Maintenance time saved
CO2 equivalent saved
Fresh water less contaminated due to pollutants
Soil less contaminated due to pollutant discharge

... with curved, lubrication-free rail guide in the tractor cabin.

... with lubrication-free insert on the trailer coupling.

... with robust energy chain for safe guidance of media in dusty and dirty environments.



... is a supplier of compact excavators, mini excavators and other small equipment and construction vehicles.
On excavators, the bearing points between the stick and the excavator bucket are exposed to high forces and harsh environmental conditions. Steel sockets are often still used here, which must be lubricated daily to ensure smooth and low-wear operation.
Four lubrication-free bearings made of high-performance polymer replace the metal bearings at the connection between the arm and the bucket. This not only saves 220 maintenance operations per year, but also saves the user high costs for lubricating grease. The risk of insufficient or incorrect lubrication is also reduced.
Lubricant cost saved
Personnel costs saved
Maintenance time saved
CO2 equivalent saved
Fresh water less contaminated due to pollutants
Soil less contaminated due to pollutant discharge

... e.g. with iglidur G polymer bearings for lubrication-free arm movement.

... with completely lubrication-free and maintenance-free heavy-duty bearings made of fibre composite material.

... with robust and corrosion-free polymer energy chain for safe guide of media.



... is the Brazilian branch of a total of 160 branches of the world-famous Heineken brewery brand.
Modern bottling plants can fill up to 70,000 bottles per hour. This process requires a large number of moving parts, such as in conveyor technology. Until now, Heineken Brazil had to regularly check and re-grease 600 radial bearings in the conveyor belts.
Polymer bearings are now used in the conveyor technology. In future, these will no longer need to be lubricated or serviced during maintenance work. Heineken Brasil is thus saving 1,560 hours of maintenance time per year and €2,815.49 in costs for the lubricants alone.
Lubricant cost saved
Personnel costs saved
Maintenance time saved
CO2 equivalent saved
Fresh water less contaminated due to pollutants
Soil less contaminated due to pollutant discharge

... with xiros conveyor rollers for lubrication-free conveyor belts.

... with maintenance-free igubal flange mounted bearings for dry operation.

... with modular and economical Apiro gearboxes.

*Assumptions for scaling:
Agricultural engineering
Construction machinery
Beverage technology