Change Language :

The control device guidance guidefast control is assembled directly on the crane girder. Like the guidefast guide trough which guides cables to the trolley (hoist), guidefast control can be fitted quickly and easily to the crane girder. The guidefast control's trough ensures that the moving arm remains securely located in the trough, even during short-term peaks in tensile strain. The roller-bearing moving arm can be shifted easily via the control device along the entire crane girder, independent of the position of the hoist.
More information:

Online:
24h